Cancel
Showing results for 
Search instead for 
Did you mean: 

how to assembly and draft one part with two configurations?

Creator
Creator

Hello,

 

Again I am having troubles with some springs... Well the thing is I have a spring that needs to be curved to fit a groove in a cylinder. I need to represent the curved spring in the assembly and the open spring in the draft. 

And I can't have multiple files for this (or multiple parts), because it is just one component and many names of files for just one part will cause some confusion to organizing the drawings.

 

Am I asking too much? I don't know if I made myself clear here, but it is such an specific problem, I could't find any solution... 

 

Thanks for your help!

1 REPLY 1

Re: how to assembly and draft one part with two configurations?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

"adjustable part" is what the doctor ordered. See this thread:

http://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/Adjustable-part/m-p/357304#U357304

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200