Cancel
Showing results for 
Search instead for 
Did you mean: 

how to change the bend direction in sheet metal

Pioneer
Pioneer

hi,

 when a sheetmetal is bended in a direction and later if i need to change the direction of the bend  how to do it please give me some suggestions.! for your refernce i have attached the screenshot

5 REPLIES 5
Highlighted

Re: how to change the bend direction in sheet metal

Phenom
Phenom

In ordered environment:

 

Click on the bend feature.

Pic1.PNG

 

Click on the Edit Definition button on the popup menu

Pic2.PNG

Click on the Bend Direction button

Pic3.PNG

 

 

 

Define a different direction and then click "Finish"

-Dylan Gondyke

Re: how to change the bend direction in sheet metal

Is it possible to change bend direction in synchronous?

 

Re: how to change the bend direction in sheet metal

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@precisionmounting wrote:

Is it possible to change bend direction in synchronous? 


 

Hi @precisionmounting,

 

Not quite as simple as ordered, but you can do it..."Detach" rotate [using the steering wheel] the flange, then "Atach" ...is what you want to do there.

 

2016-02-25 (0).png

 

2016-02-25 (1).png

 

2016-02-25 (2).png

 

2016-02-25 (3).png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: how to change the bend direction in sheet metal

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Sean, I get the detach, I get the attach, but I don't get the rotate step.

 

Edit:

I got it to work but I had to rotate it twice and move it back into position before attaching.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: how to change the bend direction in sheet metal

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Sorry, forgot to mention that part...use the steering wheel for that Bruce. [rotate & position as required]

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000