Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

how to convert autocad 2d drawing in 3d in solid edge.

PLM World Member Experimenter PLM World Member Experimenter
PLM World Member Experimenter

hi..

     I have open autocad 2d drawing in solid edge..I want to convert that drawing into 3d in solid edge.I have use solid edge ST5.

     thanks

5 REPLIES 5

Hi,   You can use the Create 3D command to create a 3D mo...

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi,

 

You can use the Create 3D command to create a 3D model with Product Manufacturing Information (PMI) in a part, sheet metal, or assembly document from 2D drawing geometry and manufacturing dimensions in a draft document. You also can use the Create 3D command to update an existing model with sketches and manufacturing dimensions.

 

For more details please refer to Solid Edge help for 'Create 3D' command.

 

Regards,

Mayuresh

Re: Hi,   You can use the Create 3D command to create a 3D mo...

PLM World Member Experimenter PLM World Member Experimenter
PLM World Member Experimenter
Thanks...

Re: Hi, You can use the Create 3D command to create a 3D mo...

Genius
Genius

Hi Guys.

 

I have tried the 'Create 3D', but it won't let me select the 2D geometry.

 

Why is this?

 

Kind regards

 

Darren

Re: Hi, You can use the Create 3D command to create a 3D mo...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Dazzie

 

 

 

I suppose that this geometry is part of a 2d view object and therefore is not selected.

Change to that view and try it there.

 

 

regards
Wolfgang

Re: Hi, You can use the Create 3D command to create a 3D mo...

Genius
Genius

Hi Wolfgang.

 

I have figured it out.

 

The geometry has to be an actual sketch, I was trying it from a draft image which is why i couldn't select anything.

 

Darren