Cancel
Showing results for 
Search instead for 
Did you mean: 

how to create holes in a sheetmetal part

Creator
Creator

how to makes holes in the small circle parts in the following sheetmetal  file given below..

2 REPLIES

Re: how to create holes in a sheetmetal part

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Not really sure what you are trying to do, but what I think you are asking is how to place holes where the sketched circles are.  If you use the Hole command, you can use the circles to locate the Holes.  Or if you just select the regions in all the circles you can just extrude a cutout to remove the material in the regions.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: how to create holes in a sheetmetal part

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @visa07,

 

Some how you have this part set as a construction body....I toggled it to a design body, then deleted the tab that resided at one of the holes, and restored the sketch. The model should then behaive as expected, adding [as @KennyG mentions] either hole features, or cutout features.

 

Here's a quick video...

 

(view in My Videos)

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000