Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

how to export (.part) to (.Dwg).???

Hello guys.?

How we can (.Asm) or(.Part) 3 d model export to (.Dwg).???

 

Electron_jaal

8 REPLIES 8

Re: how to export (.part) to (.Dwg).???

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Electron_jaal87,

 

No direct method to do this from SE,....that I know of.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP7] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: how to export (.part) to (.Dwg).???

Actually you dont know or this is impossible.???

Re: how to export (.part) to (.Dwg).???

Re: how to export (.part) to (.Dwg).???

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Electron_jaal87,

 

Well yes, that is what I meant...you cannot save a 3D model file to DWG from Solid Edge "directly"...you need to use a neutral format, such as ACIS [.SAT] file, etc.

 

Capture.PNG

 

There is also, this 3rd party app [Add-In].... http://www.sycode.com/products/dwg_export_se/ 

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP7] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: how to export (.part) to (.Dwg).???

Sure special result

Re: how to export (.part) to (.Dwg).???

Phenom
Phenom

In solid edge you need to use "save as translated" and choose .sat format.

In AutoCAD you need to use the command "import".

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user

Re: how to export (.part) to (.Dwg).???

Phenom
Phenom

@SeanCresswell,

What about the approach of Imics "https://www.youtube.com/watch?v=5v0GL1jJNe4" Solid Edge - Save as dxf from model !
It works for 2D models with [ST5;ST8]

 

Many thanks to Imics for the very good tips and triks...

Re: how to export (.part) to (.Dwg).???

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@YD, yes ageed, the things @Imics comes up with are truely amazing.....however, I think the OP was specifically looking for 3D AutoCAD [DWG or DXF] output from Solid Edge, rather than 2D.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP7] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000