Cancel
Showing results for 
Search instead for 
Did you mean: 

how to print a watermark in the draft sheet?

Creator
Creator

Hello!

 

I want to make a watermark, that only show up when printed. I'd like to do that to show an expiration date for the drawing (by the way, if anyone knows how to make a code to create an expiration date let me know Smiley Happy ).

Is it possible?

 

Thanks,

 

Bruna

 

 

 

2 REPLIES

Re: how to print a watermark in the draft sheet?

Esteemed Contributor
Esteemed Contributor

Hi there @Brunapz,

 

Not directly within Solid Edge, but it should be available in "most" printer properties.......it would be a nice feature to have as part of SE though, especially when saving a draft as PDF. [currently not available to Free2D users]

I think this is an existing ER [Enhancement Request], but I'll check....and file one, if it isn't.

 

04072016_0943.PNG

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP6] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: how to print a watermark in the draft sheet?

Solution Partner Genius Solution Partner Genius
Solution Partner Genius
It is possible to let the printer watermark the drawing, or a PDM system.
What I do is I put the text in a layer and I can then hide or show the layer depending on the use.