Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

how to sweep a pipe

Valued Contributor
Valued Contributor

i want to sweep a circular profile along a path. the start of the circular profile is different to the end.

 

see image and part file attached. 

Capture.PNG

Regards,

MagRiz
(ST9 User Est 01.18)
5 REPLIES 5

Betreff: how to sweep a pipe

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz

 

 

 

for Different Cross Sections (Multiple Sectrions) along a Sweep the path must be Tangent Continous, what is not given for Your path.

So is it possible to create a filled for the corner or should it be as drawn?

 

A sharp edge within the path only is possible for a single constant section

 

regards
Wolfgang

Betreff: how to sweep a pipe

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz

 

 

 

and here are picture from what about I have said before:

 

20180829_1054.png20180829_1055.png

regards
Wolfgang

Betreff: how to sweep a pipe

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz

 

 

PS.: for Sweeping feature only one closed profile is allowed so You can not create the wall thickness in one step together with the sweep.

But I have seen, that You have a constant wall thickness of 4.5mm so just create a Thinwall Feature afterwards!

 

regards
Wolfgang

Betreff: how to sweep a pipe

Valued Contributor
Valued Contributor

@hawcad

Thanks thats perfect. the problem was that i didnt have a fillet. i assumed it would apply an appropriate bend. 

Regards,

MagRiz
(ST9 User Est 01.18)

Betreff: how to sweep a pipe

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz

 

 

welcome, and as said, sharp corner only works for one section, but not for multiple.

 

regards
Wolfgang