Cancel
Showing results for 
Search instead for 
Did you mean: 

import a x_t file from Inventor

Valued Contributor
Valued Contributor

Hi all,

I've receved a x_t file of an assembly and I want to open it. When I try to do so, it dosn't open the file, only loading the SE program and tha stops.

Can anyone tell me if there is a certien action i have to do one i try to open a file from Inventor?

 or maybe when i try to save a file of inventor as a x_t file?

I've read that Inventor fikes comes with a lock file???

Thx

12 REPLIES 12

Betreff: import a x_t file from Inventor

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Shahar1

 

 

 

do You have the possibility to upload this file?

 

Or can You show the file properties and file size info?

 

 

regards
Wolfgang

Betreff: import a x_t file from Inventor

Valued Contributor
Valued Contributor

I am sorry, but I cant upload it, its another company's product.

i have attached  pic file of my file info as requested

Thx

Re: import a x_t file from Inventor

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Are you double-clicking the file in Windows Explorer ?

 

Re: import a x_t file from Inventor

Valued Contributor
Valued Contributor

No I got it by mail. My system operates with win7

Re: import a x_t file from Inventor

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

So are you opening it from the mail program?

 

Save the attachment to a known folder and then start Solid Edge.

In Solid Edge, press Ctrl+O and then navigate to the folder.

In the File Open dialog, change the file type filter to Parasolid (x_t) and select the saved file.

Does it show a 'Pick Template' dialog, select a 'Assembly' template and click OK.

Does that translate and open the Parasolid in SE ?

 

Re: import a x_t file from Inventor

Valued Contributor
Valued Contributor

First thank you for the detailed answer!

Did it already and after choosing the Assembly template, it  just dosn't show anything. It stays in the SE "home page".

Re: import a x_t file from Inventor

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Does it show a marquee message saying 'converting parasolid entities...' or something like that ?

 

Re: import a x_t file from Inventor

Valued Contributor
Valued Contributor

No nothing at all.

I've attached a generic asm file out of Inventor so you can try it on your system.

BDW I have SE ST1 (yes, an antique I know)

Thx

Re: import a x_t file from Inventor

Phenom
Phenom

Your problem is possibly that the x_t file is not a version that you can import.

Open an assembly in solid edge, then go to save it as an x_t. Click the Options button and see what is the latest parasolid versions you can export. It will possibly be something like 13 or 14, maybe even lower.

Then ask your Inventor user to export as that version.

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.