Cancel
Showing results for 
Search instead for 
Did you mean: 

importing and converting 2d files to 3d file

Dear All,

 

I would perform a construction drawing by starting to 3d model. Is possible to import the 3d model and create the various view an the quote them?


Regards

S

3 REPLIES

Re: importing and converting 2d files to 3d file

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Stefano_Milani,

 

Yes.....look for "View Wizard"....then use "Callout" annotation text, using the "Property Text" command to access the metadata from the connected model.

 

This from the HELP file....[View Wizard]

https://docs.plm.automation.siemens.com/tdoc/se/109/se_help/#uid:index#goto:drawing_productionSmiley Tonguertvw1h  

 

This from the HELP file....[Callout]

https://docs.plm.automation.siemens.com/tdoc/se/109/se_help/#uid:index#goto:annotations:calout1h 

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP1] Classic [x3 seats]
Windows 10 - Quadro P2000

Re: importing and converting 2d files to 3d file

I'm sorry but I wrong the title of the post. I think that you understand my request.

I try to go to home but I can't find  the "view assistant". 

From the siemens documentation I understand that is possible to import only Solidedge 3d model? It's true?

I specified also that I have solidedge 2d FREE software, not the full software.

 

Thanks

Best regards

Stefano

Re: importing and converting 2d files to 3d file

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Stefano_Milani,

 

Ah, OK.....you cannot handle anything with "3D" files in Free 2D.

Not even when viewing "Draft" files created from the full product.....and you are correct, the draft environment will only work with Solid Edge 3D files.....however, you can import other [as long as they contain 2D data] formats into Free 2D. [I believe DWG, DXF & IGES]

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP1] Classic [x3 seats]
Windows 10 - Quadro P2000