Cancel
Showing results for 
Search instead for 
Did you mean: 

inactivate assembly when opening?

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

At one time when opening a assembly through open. You could chooses whether to open it inactive or activate. I see you no longer can.  I typically don't open them this way. But, one of our designers trying to open a big assembly. Was showing how you could inactivate when opening and notice it was no longer available. when was this removed and why?

7 REPLIES

Re: inactivate assembly when opening?

Gears Phenom Gears Phenom
Gears Phenom

Open the options when you are in an assembly and look at:

options.png

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user

Re: inactivate assembly when opening?

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

thanks, got it

Re: inactivate assembly when opening?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

So the open dialog in ST8 no longer contains the options shown in the attachment?

Bruce Shand
ST10 MP7 - Insight - Win10 - K4200

Re: inactivate assembly when opening?

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

Well i'm still on ST7 and the image is the same on ST7. I just had a lap of memory..lol Old age...

Re: inactivate assembly when opening?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Tell me about it.

And that was an ST7 screen shot.

Bruce Shand
ST10 MP7 - Insight - Win10 - K4200

Re: inactivate assembly when opening?

Siemens Phenom Siemens Phenom
Siemens Phenom

@bshand wrote:

So the open dialog in ST8 no longer contains the options shown in the attachment?


 

Yes, they are just presented slightly differently I believe:

 

open1.png

 

Hitting the 'More...' button then brings up these options:

 

open2.png

 

Greg

Re: inactivate assembly when opening?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Thanks, Greg.

Bruce Shand
ST10 MP7 - Insight - Win10 - K4200