Cancel
Showing results for 
Search instead for 
Did you mean: 

insert assembly copy is not supported in family of assembly files

Pioneer
Pioneer

Does anyone have any idea why I get this error message ?

15 REPLIES 15

Re: insert assembly copy is not supported in family of assembly files

It is not possible to place a assembly copy into a family of assembly if you haven't check the 'Apply edits to all members'.

Naamloos.png

-------
Daniël Schuiling

Re: insert assembly copy is not supported in family of assembly files

Pioneer
Pioneer
well that option is un-checkable for the assembly I have

Re: insert assembly copy is not supported in family of assembly files

Hmm, do you even have a family of assembly?
Otherwise it should be checkable/not greyed out.
-------
Daniël Schuiling

Re: insert assembly copy is not supported in family of assembly files

Pioneer
Pioneer
one part has a family of parts ... thats the reason I need it

to explain real quick what I need
I have the following:
Part1 - form1 - drawing
Assembly1 which contains Part1 - form1 - assembly drawing
and finally
Assembly2 which contains Assembly1 which in turn contains Part1 - form2 - assembly2 drawing

the problem that I have here is that the first part will be riveted on the final assembly but the drawings of that part until the final assembly need to have it un-riveted

Family of parts works fine in making 1 part with 2 shapes but that intermediate assembly kills me

Re: insert assembly copy is not supported in family of assembly files

Why not just place part 1 - form 2 in the 2nd assembly?
Did you populate the part family?
-------
Daniël Schuiling

Re: insert assembly copy is not supported in family of assembly files

Pioneer
Pioneer

part1 is in the assembly 1

so a tree would look like this in the brackets I will write the form I need of part1 at each stage
Assembly2 (form2)
-Assembly 1 (form1)
--part1 (form1)

Re: insert assembly copy is not supported in family of assembly files

I'm lost, could you upload a video what you want.
-------
Daniël Schuiling

Re: insert assembly copy is not supported in family of assembly files

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

You can't link in Family of Assy last time i used it

Re: insert assembly copy is not supported in family of assembly files

Siemens Phenom Siemens Phenom
Siemens Phenom

@DanielMCMLXXXII wrote:
I'm lost, could you upload a video what you want.

 

I'm confused too - could you not make Assembly 1 the family of assemblies file with two members, one with part 1 form 1 and one with part 1 form 2? Then to make the drawing of assembly 1 with form 1, use the FOA member that contains part 1 form 1 for the drawing. Then for assembly 2, place assembly 1 into it using the member that contains part 1 form 2, which would then give you Assembly 2 containing assembly 1 using part 1 form 2.

 

Greg