Cancel
Showing results for 
Search instead for 
Did you mean: 

insert flat pattern in assembly

Genius
Genius

is it possible to insert into an assembly the flat pattern of a sheet metal file? 99% of time only need formed view.  I can create a new part file and insert part copy and flatten as part of the part copy command. Can also create a Family of Parts with 2 different files where i unbend the part. However, I am interested if there something more direct and simple I am missing?

 

Thanks,

Cory M
Solid Edge ST10
ST10 Cert
4 REPLIES 4

Re: insert flat pattern in assembly

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Yes, absolutely. The key is adjustable part, in this case you store two states in same part.

 

FOP would be nice if we could store different states in same part without populating members. Unfortunately SE doesn't support this workflow...

 

Here is a video about steps:

 

BR,

 

Imics
http://solidedgest.wordpress.com/

Re: insert flat pattern in assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Imics  Wow! Never considered the use of a suppression variable in an adjustable part.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: insert flat pattern in assembly

Genius
Genius
lmcis very impressive! worked flawlessly. Suppression variable will be tried on a few more applications. Thank you
Cory M
Solid Edge ST10
ST10 Cert

Re: insert flat pattern in assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Please mark @Imics' answer as the solution.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200