Cancel
Showing results for 
Search instead for 
Did you mean: 

insert or modify special character for arc length?

Gears Phenom Gears Phenom
Gears Phenom

I'm pretty sure the answer to this is no, but the arclength or chordlength special character symbol in edge. It's too big, doesn't look right, and really takes up too much room and looks like crap in my opinion. Does anyone know of any way to change it, or to insert a special character that i can use to replace it when I need to place it as a superfix on a dimension? Even if I need to use the symbols and values instead of grab from the special characters button, as long as I can put it as a superfix I'd be happy. Like for instance solid works' version looks way better. Below I've included snips of each to show the difference here.

 

arclength1.JPGSolidWorksarclength2.JPGSolid Edge

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"
9 REPLIES 9

Re: insert or modify special character for arc length?

I don't know about a superfix, but I know that when I try and dimension an arc with a non-constant radius, I get a dimension that looks a lot like a radius, only it has the letter "L" in front of the number instead of the letter "R".  Is that good enough, or are you trying to get it without a letter and a superfix special character in particular?

Re: insert or modify special character for arc length?

Gears Phenom Gears Phenom
Gears Phenom

@TimSchleusenerNo we're not talking about the same thing here dude. I'm talking about an arc length dimension and how I want the symbol that designates it to take up less space than it does. But thanks for trying to help.

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: insert or modify special character for arc length?

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Wow. Somebody who likes "pretty" drawings... Smiley Wink

 

Did you try to use caharacter map?

Here is a short video about steps. I used "Arial unicode MS" and it looks better than original!

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: insert or modify special character for arc length?

Gears Phenom Gears Phenom
Gears Phenom

You're a gosh dang magician @Imics, and a national treasure. Whatever nation you're in at any given time. You should be guarded like the hope diamond littered with state secrets.

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: insert or modify special character for arc length?

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

This is a great, huge, perfect exemplary for 'Out of the Box Thinking' !!

Stupendous video @Imics !!!

 

 

Re: insert or modify special character for arc length?

Gears Phenom Gears Phenom
Gears Phenom

@nominus38, my friend, I'm only an Edger... not more.

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: insert or modify special character for arc length?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Pretty good, @Imics. If you want the symbol a little closer vertically with the dim text you can modify the "line spacing" in the dim properties.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: insert or modify special character for arc length?

Gears Phenom Gears Phenom
Gears Phenom

An international treasure, indeed.  And excellent to remember to Save Settings.


____________________________________
--Scott Wertel, P.E.

Re: insert or modify special character for arc length?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

As always... Outstanding!

 

Ota