Cancel
Showing results for 
Search instead for 
Did you mean: 

install SETUP and MSI SETUP?

Valued Contributor
Valued Contributor

hi all
Is there a difference between installing Edge in Setup and installing in msi? ...

5 REPLIES

Betreff: install SETUP and MSI SETUP?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee

 

 

 

I think if You use the right command options for the MSI call then there will be no difference.

 

I suppose that finally the Setup.exe will not do anything different.

 

regards
Wolfgang

Betreff: install SETUP and MSI SETUP?

Siemens Phenom Siemens Phenom
Siemens Phenom

Installing using setup.exe will install any prerequisites.

 

Installing using .msi will *not* install any prerequisites. 

Betreff: install SETUP and MSI SETUP?

Valued Contributor
Valued Contributor

Thank you. haw cad & Uk Dave
What are you talking about as a prerequisite?

Betreff: install SETUP and MSI SETUP?

Siemens Phenom Siemens Phenom
Siemens Phenom

On the Solid Edge install media if you browse to the "Solid Edge" folder, under this you will see the folder "ISSetupPrerequisites".  These are the prerequisites that Solid Edge installs.

 

If your system does not have the required software prerequisites, the Solid Edge setup.exe will then attempt to install those prerequisites from within this "ISSetupPrerequisites" folder.

 

In this " ISSetupPrerequisites" folder are the following software:

 

  • Key Shot
  • .NET 4.5
  • Silverlight
  • Visual C++ 2015 Redistributable

Betreff: install SETUP and MSI SETUP?

Valued Contributor
Valued Contributor

Thankyou~