Cancel
Showing results for 
Search instead for 
Did you mean: 

installation of ST9

Experimenter
Experimenter

Can the student version of ST9 be installed on Windows 7 home edition

4 REPLIES

Re: installation of ST9

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes, ST9 Student Edition will install on Windows 7 Home.

Re: installation of ST9

Experimenter
Experimenter
Thanks for that,
my problem is that the initial splash screen comes up when selecting ST9 but it just hangs without actually loading

cheers

Re: installation of ST9

Siemens Genius Siemens Genius
Siemens Genius

install the latest GPU driver.

Re: installation of ST9

Siemens Phenom Siemens Phenom
Siemens Phenom

Manually create the following registry keys to force the software to use backing store as the default display setting:

 

[HKEY_CURRENT_USER\Software\Unigraphics Solutions\Solid Edge\Version 109\PrefSets\Options-View]
"AutoConfigure"=hex:06,00,00,00,00,00,00,00,00,00,00,00,00,00,00,00
"BackingStore"=hex:02,00,00,00,00,00,00,00,02,00,00,00,00,00,00,00