Cancel
Showing results for 
Search instead for 
Did you mean: 

installing problems

Not applicable

Hello.
I tried to install solid edge ST5, but it was interrupted because my pc works on windows xp. So, my question is, if I change pc with one with the characteristics required, can I used the same student licence?? Can I restart the same download???

3 REPLIES

Re: installing problems

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Hi there,
Yes, it is acceptable to re-use your downloaded license file (.txt) & application (.exe)...it is easily transferable via external storage, to your other PC(s) running on Windows-7.
(right mouse click on install app, choose "run as administrator")
While not certified for Windows-8, I know of working installs. Next release will be fully compliant.
HTH.

Sean Cresswell
Streetscape Limited (NZ)
-
Sent from my Samsung Galaxy NoteII using Tapatalk 2.
-
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: installing problems

Not applicable
I tried to install on Windows-7 Home Premium 64-bits. The application not run. Why?

Re: installing problems

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
When installing on Windows 7, follow these suggestions:
* Install to a location outside of "C:\Program Files" (example: "C:\Solid Edge\")
* Run Setup.exe by clicking your right mouse button and select "Run as Administrator"


Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com