Cancel
Showing results for 
Search instead for 
Did you mean: 

insulation fill/hatch - overlapping 'S' shape

Genius
Genius

Is there a fill pattern to show the common type  for insulation of an overlapping 'S' shape?

 

This is a fairly universal pattern that is well understood, but I have not seen it in Solid Edge. There is the radial pattern, so it seems that hatches are no longer limited to just straight lines.

 

2 REPLIES

Betreff: insulation fill/hatch - overlapping 'S' shape

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @pmckay

 

 

 

AFAIK there will be no hatch/fill style other than the linear one and the wood fill.

 

This would be a big enhancement if we would be able to use fill/hatch patterns with more "complex" (not really complex, isn't it) geometry for materials like concrete (better than now), isolation, etc.

 



regards
Wolfgang

Betreff: insulation fill/hatch - overlapping 'S' shape

Genius
Genius
Thanks @hawcad. Yes, it's a bit embarrassing when you tell a client that, umm, no I can't do what AutoCad and Solid Works can do....