Cancel
Showing results for 
Search instead for 
Did you mean: 

is my sketch completely dimensioned?

Experimenter
Experimenter

Hi there!

 

I'm using Solid Edge 2D Drafting ST6. Is there a way to notice, that my sketch is completely dimensioned? Some time ago I have been working with CATIA; it's sketching module showed different line colors when the sketch was either been under, correctly or overdimensioned.

 

Thanks in advance!

1 REPLY

Solid Edge also has that capability in the sketch environ...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Solid Edge also has that capability in the sketch environments of the 3D modes, but I do not believe it is available in Draft.  The closest tool you can use is the Relationship Assistant.  When invoked, there are two parts to it.  One part "auto constrains" elements while the other part (Show Variability) will tell you when you are partially/fully constrained.



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com