06-03-2017 09:56 AM
Hello, my son is interested in downloading the student version of Solid Edge but we have a mac and I am wondering if there is a version for macs? All I see in the system requirements is windows... help!
06-05-2017 07:38 AM
SE will not install on the MAC OS. There are users running SE on MACs however. It is my understanding that you need a "Boot Camp" like software that allows you to boot the machine into either the Apple OS or a Windows environment. Once booted in the Windows environment you can install and run SE...
REF: https://support.apple.com/en-gb/HT201468
Good luck.