Cancel
Showing results for 
Search instead for 
Did you mean: 

is sold edge avail for Macs?

Experimenter
Experimenter

Hello, my son is interested in downloading the student version of Solid Edge but we have a mac and I am wondering if there is a version for macs?  All I see in the system requirements is windows... help!

1 REPLY 1

Re: is sold edge avail for Macs?

Gears Phenom Gears Phenom
Gears Phenom

SE will not install on the MAC OS.  There are users running SE on MACs however.  It is my understanding that you need a "Boot Camp" like software that allows you to boot the machine into either the Apple OS or a Windows environment.  Once booted in the Windows environment you can install and run SE...

 

REF: https://support.apple.com/en-gb/HT201468

 

Good luck.

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7