Cancel
Showing results for 
Search instead for 
Did you mean: 

isometric view dimension

Valued Contributor
Valued Contributor

Hello everyone
I want to fill the isometric view with frame spacing dimensions.
It's not important, so just mark the interval.
However, it is difficult to dimension the isometric view.

To use the PMI view ....
I think it is a waste of time because it seems to do one more thing.

Is not there a good way?

DIMENSION.png

6 REPLIES

Re: isometric view dimension

Phenom
Phenom

https://docs.plm.automation.siemens.com/tdoc/se/109/se_help/#uid:dim3d1h

 

 

Bob Henry
REH Technical Consulting
Canonsburg, PA 15317

Re: isometric view dimension

Valued Contributor
Valued Contributor

good Infomation

Thankyou~

Re: isometric view dimension

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee

 

 

 

You can use Smart Dimensions only for dimensioning within apictrual view.

 

Please check options for 3D dimensioning for non ISO views

 

 



regards
Wolfgang

Re: isometric view dimension

Valued Contributor
Valued Contributor

hi~ hawcad

Expert mode? What are you talking about?
pmi view seems to work twice ..
I do not like it.

Re: isometric view dimension

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee

 

 

see attached video.

And take care when I have created the new view somehow in space and retrieve the frist dimensions which are wrong!

Until I change the option for that view to "Retrieve 3D diemensions"

 

Then everything is OK.

 

This setting is OK for any standard picture views like ISO and so on.

but not for any user define

(view in My Videos)
d views

 

 



regards
Wolfgang

Re: isometric view dimension

Valued Contributor
Valued Contributor

Good morning hawcad
Very useful video.
The arbitrary view is not checked.
Thank you.