Cancel
Showing results for 
Search instead for 
Did you mean: 

item numbers

Experimenter
Experimenter

I am updating the old draft files, which are ballooned and have BOM. I need to change the item numbers in BOM and change the ballooning pattern (same pattern for each draft file)

 

if I do the auto- ballooning first for all views, and then change the item numbers, it takes a lot of time.

 

And if I update the BOM first and then do the auto ballooning, it will save much time, but the item numbers get changed by doing this.

 

please advise the suitable method

2 REPLIES

Betreff: item numbers

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Jag22

 

obviously it is due to the late time we have here, but I can not follow You beyond the first line.

 

So if possible, can You explain it a little more detailed, maybe accomplished by pictures or video.

 

I think this would help me to help You!

 

 

regards
Wolfgang

Re: item numbers

Gears Phenom Gears Phenom
Gears Phenom

@Jag22

 

if you need to retain the item numbers you need to define them in the assy and then in the draft, there is an option to use assembly defined item numbers...


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7