Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

keyshot hang when I click "keyshot render" button in Assembly Environment

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

ST 8, MP11

 

keyshot hang when I click "keyshot render" button in Assembly Environment

 

1. open a assembly

 

2. click "keyshot render"

 

3. successfully opened (First = success)

 

4. Close "keyshot"

 

5. Reopen keyshot (use keyshot render)

 

6. keyshot freeze (second = hang. keyshot logo is appeared but stop)

 

 

how can I solve it?

1 REPLY 1

Re: keyshot hang when I click "keyshot render" button in Assembly Environment

Legend
Legend

Hi @jsy,

 

I had a similar issue when I updated my workstation to Windows 10. MY VAR helped me with the issue and it turned out that Keyshot 5 and Windows 10 had problems working together. After I updated Keyshot to Keyshot 6, the problem disappeared and everything works like it should now. The update is free when you have Solid Edge.

 

If you still have Keyshot 5, you can update to Keyshot 6 HERE