Cancel
Showing results for 
Search instead for 
Did you mean: 

keyshot - update view

Phenom
Phenom

What do I do wrong?

I want a render from an assembly in defferent positions. I make pasition one in SE and send it to keyshot. The render:

karren.jpg

Then I fo back to SE and move one of both sets to get in one line. Now I send this again to keyshot, the result:

Kar1+2.112.jpg

Wtf...

the old position is still there! 

Because I made groups per material it is not a "one click operation" to hide the parts that I don't need.

 

So: How can I tell Keyshot from whitin SE that this are the same parts, just in an other position?

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user
2 REPLIES 2

Betreff: keyshot - update view

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Joris

 

 

 

just for verification, but You hit the Update Keyshot button?

 

And which Keyshot version are You using.

I have seen better cooperation with ST10 and Keyshot 7.xxx

 

 

 

regards
Wolfgang

Betreff: keyshot - update view

Phenom
Phenom

I just hit the "update keyshot" button.

SE ST10 MP 5

Keyshot 7.2

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user