Cancel
Showing results for 
Search instead for 
Did you mean: 

laptop/notebook for Solid Edge

Experimenter
Experimenter

I travel nonstop and work in industrial environments.  What will be the best, reasonably affordable (under $1,500.00) notebook for using Solid Edge ST7.  I receive some customer files that are 65mb or so that I have to manipulate.  Any hardware suggestions will be appreciated as well.  I currently use an ASUS N55S I7 processor with 8gb ram.  It works ok until I get files that are 50mb or so.  Then it gets sluggish.  It is 3 years old and well-traveled (meaning beat all to heck). 

3 REPLIES
Highlighted

Re: laptop/notebook for Solid Edge

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

I've been angling towards a Surface Pro3......and just recently @BobMileti posted on his recent activity on one.....

http://community.plm.automation.siemens.com/siemensplm/board/message?board.id=solid-edge-forum&messa...

 

[and his video showing an 1000 part assembly]

http://screencast.com/t/2Lha1VIF

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: laptop/notebook for Solid Edge

Experimenter
Experimenter
thanks for the info. I was doing a bit of dreaming about the surface.

Re: laptop/notebook for Solid Edge

Gears Phenom Gears Phenom
Gears Phenom

Just out of curiosity, has anyone tried Solid Edge on a Lenovo Yoga 2?

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1