Cancel
Showing results for 
Search instead for 
Did you mean: 

lbm to lbs

On my title blocks I have a weight listed that parapetrically links to the mass of the model in the drawing.  I have one customer that is KILLING me that they want to see LBS instead of LBM.  I realize that LBM is a mass unit of measure, but I do not know how to make it where it doesnt show the LBM suffix.  Is there a way to do this?

 

Capture.JPG

Owner: Scott Lester Drafting & Design
Designer: Rotork Instuments
3 REPLIES 3

Re: lbm to lbs

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

"/NU" after the property name.  Ex. "%{Mass/NU} LBS"



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: lbm to lbs

I figured it was a code to put in like that!  I knew you could put things like /@2 after the property to adjust the decimal points and whatnot.  Is there a list of codes like that somewhere I can print to reference for future use?

Owner: Scott Lester Drafting & Design
Designer: Rotork Instuments

Re: lbm to lbs

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

https://docs.plm.automation.siemens.com/tdoc/se/109/se_help/#uidSmiley Tonguerptxt4a



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com