Cancel
Showing results for 
Search instead for 
Did you mean: 

lmtools and using groups

Valued Contributor
Valued Contributor

We are trying to use the selmd.opt file to limit (restrict) the amount of individuals from a certain group to access Solid Edge, but I think we must have something wrong with the syntax because it currently is allowing more than the alloted amount we set.  Can someone that has more experience using this option review what we have and see if they can see an error in our syntax?

 

The results of running the server status are shown below.  It shows 4 licenses being used by toolroom and 1 being used be cpfrank.  NOTE: cpfrank & toolroom = user logins, toolrm is the new group name.  

 

Here is what we currently have:

 

NOLOG UNSUPPORTED

GROUPCASEINSENSITIVE ON

GROUP toolrm toolroom cpfrank

RESERVE 3 solidedgeclassic GROUP toolrm

 

 

Flexible License Manager status on Mon 12/11/2017 08:25

[Detecting lmgrd processes...]
License server status: 27001@SEATS-SRV8
License file(s) on SEATS-SRV8: C:\SEFlex\Program\SELicense.dat:

SEATS-SRV8: license server UP (MASTER) v11.13.1

Vendor daemon status (on SEATS-SRV8):

selmd: UP v11.13.1
Feature usage info:

Users of solidedgeclassic: (Total of 19 licenses issued; Total of 19 licenses in use)

"solidedgeclassic" v109.0, vendor: selmd, expiry: 1-jan-0
floating license

 

toolroom seats-pc350 seats-pc350 (v109.0) (SEATS-SRV8/27001 1710), start Mon 12/11 4:07
cpfrank Seats-PC437 Seats-PC437 (v109.0) (SEATS-SRV8/27001 1020), start Mon 12/11 4:10
toolroom SEATS-PC417 SEATS-PC417 (v109.0) (SEATS-SRV8/27001 811), start Mon 12/11 4:21
toolroom SEATS-PC450 SEATS-PC450 (v109.0) (SEATS-SRV8/27001 105), start Mon 12/11 5:59
toolroom SEATS-PC351 SEATS-PC351 (v109.0) (SEATS-SRV8/27001 1311), start Mon 12/11 6:10

29 REPLIES 29

Betreff: lmtools and using groups

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MikeSaari

 

 

 

according to Your info file, at the moment there are all licenses in use (19 from 19 in use)

 

Maybe You have to stop all those useres once, reread the license file and then let them start again.

 

regards
Wolfgang

Betreff: lmtools and using groups

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MikeSaari

 

 

 

also the CASESENSITIVE I have never seen or used this as ON

 

 

regards
Wolfgang

Betreff: lmtools and using groups

Valued Contributor
Valued Contributor

The option file was created sometime ago and everyone should have been logged off over the weekend so I would think that the file would have been re-read, but it's entirely possible that not everyone had gotten out of Solid Edge.

Betreff: lmtools and using groups

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Did you stop and start the server from lmtools?

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200
Highlighted

Betreff: lmtools and using groups

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MikeSaari

 

 

 

 

as long as You haven't reread the licens/options files the FlexLM server will not recognize those changes in Your option file.

 

As mentioned by @bshand You also can stop and start trhe server again, but this needs all users to be logged of from SE.

ReRead can be done even if users are logged in and use SE.

So theer is not need for stopping SE.

Same is true if You change the license file, since You have got new SE licenses, etc.

Simply reread is all You need, and no stop and start.

 

 

You should be able to see the results if You do a status query in lmtools afterwards

regards
Wolfgang

Betreff: lmtools and using groups

Valued Contributor
Valued Contributor

I'm not sure why case sensitive was set to be ON.

 

Betreff: lmtools and using groups

Valued Contributor
Valued Contributor

I will try to have everyone log off, but it could be awhile.  While we wait for that, let me ask this question.  When using the "reserve" option and I set it to "3".  Does it allow the reserved group to access more than 3 if there are more licenses available?  Would we be better to use the MAX option?

Betreff: lmtools and using groups

Valued Contributor
Valued Contributor

I did perform the Reread.

 

Status
--------
Flexible License Manager status on Mon 12/11/2017 09:54

[Detecting lmgrd processes...]
License server status: 27001@SEATS-SRV8
License file(s) on SEATS-SRV8: C:\SEFlex\Program\SELicense.dat:

SEATS-SRV8: license server UP (MASTER) v11.13.1

Vendor daemon status (on SEATS-SRV8):

selmd: UP v11.13.1
Feature usage info:

Users of solidedgeclassic: (Total of 19 licenses issued; Total of 19 licenses in use)

"solidedgeclassic" v109.0, vendor: selmd, expiry: 1-jan-0
floating license

toolroom seats-pc350 seats-pc350 (v109.0) (SEATS-SRV8/27001 1710), start Mon 12/11 4:07
cpfrank Seats-PC437 Seats-PC437 (v109.0) (SEATS-SRV8/27001 1020), start Mon 12/11 4:10
toolroom SEATS-PC417 SEATS-PC417 (v109.0) (SEATS-SRV8/27001 811), start Mon 12/11 4:21
KLICKO SEATS-PC394 SEATS-PC394 (v109.0) (SEATS-SRV8/27001 2011), start Mon 12/11 4:38
toolroom SEATS-PC450 SEATS-PC450 (v109.0) (SEATS-SRV8/27001 105), start Mon 12/11 5:59
ssteinhorst SEATS-PC390 SEATS-PC390 (v109.0) (SEATS-SRV8/27001 1106), start Mon 12/11 6:00
toolroom SEATS-PC351 SEATS-PC351 (v109.0) (SEATS-SRV8/27001 1311), start Mon 12/11 6:10
pbrey SEATS-PC396 SEATS-PC396 (v109.0) (SEATS-SRV8/27001 205), start Mon 12/11 6:12
bauerk SEATS-PC391 SEATS-PC391 (v109.0) (SEATS-SRV8/27001 1908), start Mon 12/11 6:47
TATE SEATS-PC392 SEATS-PC392 (v109.0) (SEATS-SRV8/27001 1818), start Mon 12/11 7:03
rdowning SEATS-LT123 SEATS-LT123 (v109.0) (SEATS-SRV8/27001 1508), start Mon 12/11 7:11
dziemer SEATS-PC395 SEATS-PC395 (v109.0) (SEATS-SRV8/27001 613), start Mon 12/11 7:12
wehlers SEATS-PC393 SEATS-PC393 (v109.0) (SEATS-SRV8/27001 318), start Mon 12/11 7:17
jboyarski SEATS-PC398 SEATS-PC398 (v109.0) (SEATS-SRV8/27001 1207), start Mon 12/11 7:48
jjenson SEATS-LT132 SEATS-LT132 (v109.0) (SEATS-SRV8/27001 508), start Mon 12/11 7:54
shendrickson SEATS-PC397 SEATS-PC397 (v109.0) (SEATS-SRV8/27001 712), start Mon 12/11 8:02
ckrueger SEATS-PC399 SEATS-PC399 (v109.0) (SEATS-SRV8/27001 1612), start Mon 12/11 8:09
pvanzyl SEATS-LT141 SEATS-LT141 (v109.0) (SEATS-SRV8/27001 413), start Mon 12/11 8:21
NALEPINSKI SEATS-PC389 SEATS-PC389 (v109.0) (SEATS-SRV8/27001 1411), start Mon 12/11 9:22

Users of server_id: (Total of 1 license issued; Total of 0 licenses in use)

Betreff: lmtools and using groups

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MikeSaari

 

 

 

let the tollroom user log out from SE

 

See how many licenses are issued then and how many are free to use.

 

And I suppose, that if You reserve 3 lcienses for a user toolroom, and this user is logged into 3 PCs then also 3 licenses will be used.

 

Again stop all SE useres from using it, reread and se the status in lmtools.

This clearly must show 3 reservatiosn for the group toolrm

And I would suggest to turn of the case sensitive option, You can not really no the exact writing of usernames by the system.

 

 

 

 

regards
Wolfgang