Cancel
Showing results for 
Search instead for 
Did you mean: 

Betreff: lmtools and using groups

Siemens Phenom Siemens Phenom
Siemens Phenom

Keyword RESERVE does not limit the total number of licenses available.  All this does is ensure that there will be a minimum number of licenses available to the assigned group preventing other non-assigned users from accessing this reserved number of licenses.  The assigned group can still take more than what has been reserved.

 

Keyword MAX will limit the total number of licenses a group can access.  Without trying it I do not know at this time if Solid Edge supports the use of the keyword MAX.

Highlighted

Betreff: lmtools and using groups

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @uk_dave

 

 

 

good point I forgot to mention.

So we always defined several groups with their specified reservations where the total number of licenses was equal to the total number of reservations.

This prevent any group of taking more than the assigned licenses for them.

 

regards
Wolfgang

Betreff: lmtools and using groups

Valued Contributor
Valued Contributor

Thanks for the reply regarding the "reserve" option.  I kind of figured that's how it might work.  So when you say..."licenses was equal to the total number of reservations.  This prevent any group of taking more than the assigned licenses for them."  Would I be best to reserve 3 for toolrm and 16 for design engineering?

 

 

I had the toolroom users and cpfrank log out of SE.  I re-read the lisence and this is what I get.  Notice at the bottom it now says" 1 RESERVATION for GROUP toolrm (SEATS-SRV8/27001)It did not say that before.  Any idea why?

 

Users of solidedgeclassic:  (Total of 19 licenses issued;  Total of 17 licenses in use)

 

  "solidedgeclassic" v109.0, vendor: selmd, expiry: 1-jan-0

  floating license

 

    KLICKO SEATS-PC394 SEATS-PC394 (v109.0) (SEATS-SRV8/27001 2011), start Mon 12/11 4:38

    ssteinhorst SEATS-PC390 SEATS-PC390 (v109.0) (SEATS-SRV8/27001 1106), start Mon 12/11 6:00

    pbrey SEATS-PC396 SEATS-PC396 (v109.0) (SEATS-SRV8/27001 205), start Mon 12/11 6:12

    bauerk SEATS-PC391 SEATS-PC391 (v109.0) (SEATS-SRV8/27001 1908), start Mon 12/11 6:47

    TATE SEATS-PC392 SEATS-PC392 (v109.0) (SEATS-SRV8/27001 1818), start Mon 12/11 7:03

    rdowning SEATS-LT123 SEATS-LT123 (v109.0) (SEATS-SRV8/27001 1508), start Mon 12/11 7:11

    dziemer SEATS-PC395 SEATS-PC395 (v109.0) (SEATS-SRV8/27001 613), start Mon 12/11 7:12

    jboyarski SEATS-PC398 SEATS-PC398 (v109.0) (SEATS-SRV8/27001 1207), start Mon 12/11 7:48

    shendrickson SEATS-PC397 SEATS-PC397 (v109.0) (SEATS-SRV8/27001 712), start Mon 12/11 8:02

    ckrueger SEATS-PC399 SEATS-PC399 (v109.0) (SEATS-SRV8/27001 1612), start Mon 12/11 8:09

    pvanzyl SEATS-LT141 SEATS-LT141 (v109.0) (SEATS-SRV8/27001 413), start Mon 12/11 8:21

    NALEPINSKI SEATS-PC389 SEATS-PC389 (v109.0) (SEATS-SRV8/27001 1411), start Mon 12/11 9:22

    cpfrank Seats-PC437 Seats-PC437 (v109.0) (SEATS-SRV8/27001 1021), start Mon 12/11 11:24

    toolroom SEATS-PC450 SEATS-PC450 (v109.0) (SEATS-SRV8/27001 106), start Mon 12/11 11:25

    bnemec Seats-PC344 Seats-PC344 (v109.0) (SEATS-SRV8/27001 812), start Mon 12/11 11:27

    toolroom seats-pc350 seats-pc350 (v109.0) (SEATS-SRV8/27001 1711), start Mon 12/11 11:37

                1 RESERVATION for GROUP toolrm (SEATS-SRV8/27001)

 

Users of server_id:  (Total of 1 license issued;  Total of 0 licenses in use)

Betreff: lmtools and using groups

Siemens Phenom Siemens Phenom
Siemens Phenom

Because toolrm is only using two licenses, one additional license is still reserved for toolrm.

 

If no toolrm users had taken licenses then it would state three licenses reserved.

 

And yes, theoretically you could reserve [assign] all of your licenses to each of the groups such that the total of all licenses available have been reserved by various groups.  This is what @hawcad was stating.

Betreff: lmtools and using groups

Valued Contributor
Valued Contributor

Actually now that I re-look at the server status I don't think there should be one license left for the toolrm group seeing as (2) are being used by the toolroom and (1) is being used by cpfrank, and they are part of the toolrm group.

 

    cpfrank Seats-PC437 Seats-PC437 (v109.0) (SEATS-SRV8/27001 1021), start Mon 12/11 11:24

    toolroom SEATS-PC450 SEATS-PC450 (v109.0) (SEATS-SRV8/27001 106), start Mon 12/11 11:25

    bnemec Seats-PC344 Seats-PC344 (v109.0) (SEATS-SRV8/27001 812), start Mon 12/11 11:27

    toolroom seats-pc350 seats-pc350 (v109.0) (SEATS-SRV8/27001 1711), start Mon 12/11 11:37

                1 RESERVATION for GROUP toolrm (SEATS-SRV8/27001)

 

Later in the day...why does the one above say 2 RESERVATIONs for GROUP toolrm  and the one below says 2 RESERVATIONs for GROUP toolrm??  The one below that now says 3 RESERVATIONs for GROUP toolrm.  It's almost as if they are getting an extra license.

 

Users of solidedgeclassic:  (Total of 19 licenses issued;  Total of 10 licenses in use)

 

 

    jboyarski SEATS-PC398 SEATS-PC398 (v109.0) (SEATS-SRV8/27001 1207), start Mon 12/11 7:48

    ckrueger SEATS-PC399 SEATS-PC399 (v109.0) (SEATS-SRV8/27001 1612), start Mon 12/11 8:09

    pvanzyl SEATS-LT141 SEATS-LT141 (v109.0) (SEATS-SRV8/27001 1312), start Mon 12/11 13:01

    NALEPINSKI SEATS-PC389 SEATS-PC389 (v109.0) (SEATS-SRV8/27001 1411), start Mon 12/11 9:22

    toolroom SEATS-PC450 SEATS-PC450 (v109.0) (SEATS-SRV8/27001 106), start Mon 12/11 11:25

    tmueller SEATS-LT122 SEATS-LT122 (v109.0) (SEATS-SRV8/27001 323), start Mon 12/11 12:45

    toolroom SEATS-PC319 SEATS-PC319 (v109.0) (SEATS-SRV8/27001 2013), start Mon 12/11 14:32

    bnemec Seats-PC344 Seats-PC344 (v109.0) (SEATS-SRV8/27001 1713), start Mon 12/11 15:07

                2 RESERVATIONs for GROUP toolrm (SEATS-SRV8/27001)

 

Users of solidedgeclassic:  (Total of 19 licenses issued;  Total of 8 licenses in use)

 

    ckrueger SEATS-PC399 SEATS-PC399 (v109.0) (SEATS-SRV8/27001 1612), start Mon 12/11 8:09

    pvanzyl SEATS-LT141 SEATS-LT141 (v109.0) (SEATS-SRV8/27001 1312), start Mon 12/11 13:01

    NALEPINSKI SEATS-PC389 SEATS-PC389 (v109.0) (SEATS-SRV8/27001 1411), start Mon 12/11 9:22

    toolroom SEATS-PC450 SEATS-PC450 (v109.0) (SEATS-SRV8/27001 106), start Mon 12/11 11:25

    tmueller SEATS-LT122 SEATS-LT122 (v109.0) (SEATS-SRV8/27001 323), start Mon 12/11 12:45

            3 RESERVATIONs for GROUP toolrm (SEATS-SRV8/2700

 

Current option file settings

NOLOG UNSUPPORTED

GROUPCASEINSENSITIVE ON

GROUP toolrm toolroom cpfrank

RESERVE 3 solidedgeclassic GROUP toolrm

Betreff: lmtools and using groups

Siemens Phenom Siemens Phenom
Siemens Phenom

Because at some point in the license assignment "toolroom" was not able to take one of the reserved licenses and instead got granted one of the remaining  unreserved licenses, most probably because when the second toolroom user asked for a license all three reserved licenses at that time were in use.  Then one of the reserved licenses was later returned while the fourth user session was still running.  At this point Flex isn't going to magically figure out that the fourth user should now be flipped back to a reserved but instead will see that the previously reserved is now returned and as such will make the previously used reserved once again available as a reserved.

 

You also have to take into consideration that when you pull these license stats that these are a snapshot at that moment in time and do not show the historical assignment of the licenses.

Betreff: lmtools and using groups

Valued Contributor
Valued Contributor

That makes sense.  I have to apologize for my limited knowledge of how the lisencing works.  Given what you said, I'm trying to figure out what makes the most sense for setting this up .

 

We have a pool of 19 licenses, 16 of which design engineering "owns", and 3 that the toolroom "owns".  We have certain "power users" and we have the "occasional" user and as you've seen we run into the toolroom using too many.  The RESERVE option doesn't work that great if I just include design engineers and toolroom because that would limit our use and we couldn't pull a license while in our conf rooms unless I add our conf rooms to the DE group.  

 

I'm thinking the MAX option might be our best solution, but before I make a decision, does anyone know how the TIMEOUT option works?  If I set it for 1 hr and the user gets "timedout", will they still be able to save their work?  Do they have to wait for a license to become available in order to save their work?

Betreff: lmtools and using groups

Siemens Phenom Siemens Phenom
Siemens Phenom

Although TIMEOUT is a Flex option, currently Solid Edge does not support using TIMEOUT.

Betreff: lmtools and using groups

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MikeSaari

 

 

 

so solve it the other way round.

Create a group of users for a DESIGN and RESERVE them 16 licenses.

To prevent all designer occupying all licenses You also should RESERVE 3 for the toolroom

 

So You have reserved all licenses for adequate users.

 

regards
Wolfgang

Betreff: lmtools and using groups

Siemens Phenom Siemens Phenom
Siemens Phenom

Except that would then require putting all non-toolroom users into the design group which is what @MikeSaari stated he did not want to do.