Cancel
Showing results for 
Search instead for 
Did you mean: 

main assemblt hide automaticaly

Experimenter
Experimenter

all sub assem showing but above main assem is hidden .i triad to showall ,activate option but main assem not shown

4 REPLIES 4

Re: main assemblt hide automaticaly

Gears Phenom Gears Phenom
Gears Phenom

was this an imported assy?  its possible that you have no design bodies,  only surfaces...  surfaces do not show at the assy level by default you will need to show them manually.

 

has this assy ever "worked" for you?

 

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Re: main assemblt hide automaticaly

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Right mouseclick in the screen

Tick show all for everything

Showall.JPG

Re: main assemblt hide automaticaly

Experimenter
Experimenter

I TRIED THE SURFACES ON BUT STII   NOT SHOWN

 

ONCE I OPEN SUB ASSEM FROM SAME .IT OPEN AND SHOWN EASILY 

ONLY MAIN ASSEM NOT SHOWING 

Re: main assemblt hide automaticaly

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Are you in design mode?Design.jpg