Cancel
Showing results for 
Search instead for 
Did you mean: 

mass-delete custom properties

Valued Contributor
Valued Contributor

I need to delete some custom properties from several hundred files. Using the property manager I can delete the value of the property but the property itself remains in each file.

Is there a way to obtain this, other than open and edit every single file?

____________________________
http://www.stimarchetti.it
Design of automation
4 REPLIES

Re: mass-delete custom properties

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

I can only think of a macro, especialy since you have several hundred files.

 

Re: mass-delete custom properties

Valued Contributor
Valued Contributor

Sadly I'm not able to create code....

____________________________
http://www.stimarchetti.it
Design of automation

Re: mass-delete custom properties

Legend
Legend

@Alessandro

 

Although an old tool, it still does the job as it should do (and even more); Property Remapper.

http://barhamsoftware.com/SE_Tools/index.htm

 

Only thing to do with this tool is to install the View & Markup program as it requires some 32-bit components which do not install with the vanilla SE installation.

 

See also https://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/propseed-and-changed-property-types...

 

 

--------------------------------------------------
Marc Boom
marc.boom@outlook.com

Re: mass-delete custom properties

Valued Contributor
Valued Contributor

This program works out of the box!

 

Nice, and thank you very much!

____________________________
http://www.stimarchetti.it
Design of automation