Cancel
Showing results for 
Search instead for 
Did you mean: 

metric AND imperial dimension

Valued Contributor
Valued Contributor

Is it possible to display both metric (2920 mm) and imperial (Inches 9'-6 15/16) value in 1 dimension on a drawing view?

5 REPLIES 5

Re: metric AND imperial dimension

Phenom
Phenom

Yea if you right click on the dimension and go to properties for the dimension, there's a page called Secondary Units where you have the options to add another unit and how you want it displayed.

Re: metric AND imperial dimension

Phenom
Phenom

Hi,

 

You could display the secondary dimensions and you could create a new template containing the two dimensions, so that you get them with every new dimention.

 

mm_inch.JPG

 

Yasser

Re: metric AND imperial dimension

Honored Contributor
Honored Contributor

I think the limiting factor is Tolerance. You can only display tolerance values in the main units. The alternate units can only display a nominal value.

Re: metric AND imperial dimension

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Pretty sure tolerances display the same value as the primary but converted into the secondary units.

tolunits.JPG

 

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: metric AND imperial dimension

Phenom
Phenom

Additional Info...

 

Dual_Units.JPG