Cancel
Showing results for 
Search instead for 
Did you mean: 

model difference from draft with long sweep help ST7

Genius
Genius

I am having trouble getting a draft file to display a model in an acceptable manner.

Model is of a pair of wires, 1600mm long, outer insulation 1.5mm dia.

2 sketches used to create path & profile. Loft command used to generate protrusions. Model appears correct, but draft file is rather course in depiction of model.

 

Any suggestions would be great.

 

Gary Dinges | Mechanical Design Engineer | New Product Development Emerson Climate Technologies | Therm-O-Disc, Inc.| 1320 South Main Street | Mansfield | OH | 44907 | USA T +1 419 525 8554 gary.dinges@emerson.com

6 REPLIES 6

Re: model difference from draft with long sweep help ST7

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I was able to get better results if I changed the sweep options to "no merge" in the part.

I thought setting the simplify b-spline edges to "never" in the drawing view would have done the trick but no.

LMGi
www.TLMGi.com

Re: model difference from draft with long sweep help ST7

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Wow, that is an odd one......the draft doesn't match the model representation at all.

If you haven't already, I'd be inclined to send that into GTAC for review.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: model difference from draft with long sweep help ST7

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Gary,

You really need to report this one to GTAC. It does the same (or similar) in ST8.

Cheers

Mark

Re: model difference from draft with long sweep help ST7

Genius
Genius

Using the No Merge setting has helped.

Discovered another symptom. The part represents a pair of wires, the longer I make the pair of wires, the worse the deformation becomes. Some pictures attached of longer lengths.

I will send this to GTAC today.

Thanks for the help.

 

Gary Dinges | Mechanical Design Engineer | New Product Development Emerson Climate Technologies | Therm-O-Disc, Inc.| 1320 South Main Street | Mansfield | OH | 44907 | USA T +1 419 525 8554 gary.dinges@emerson.com

Re: model difference from draft with long sweep help ST7

Genius
Genius

GTAC incedent # 7444338

 

Gary Dinges | Mechanical Design Engineer | New Product Development Emerson Climate Technologies | Therm-O-Disc, Inc.| 1320 South Main Street | Mansfield | OH | 44907 | USA T +1 419 525 8554 gary.dinges@emerson.com

Re: model difference from draft with long sweep help ST7

Phenom
Phenom

The draft will display more correctly if the VHL tolerance is actually set to 1 in the Advanced options tab of the view. Anything greater than 1 and the draft looks much worse.

-Dylan Gondyke