Cancel
Showing results for 
Search instead for 
Did you mean: 

need to reinstall solidedge on another computer

N/A

Hi!
I had previously installed solid-edge (october 2011) on a netbook. Now I bought a new more capable computer and need to install it again. I registered three times for a new license but did not get any reply. How can I do to install solid-edge again? please help. Thank you.

1 REPLY

Re: need to reinstall solidedge on another computer

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Hi Marco,

If you have a copy of the ".exe" install file, but only require the license.

http://dl2.plm.automation.siemens.com/solidedge/SolidEdgeV104ENGLISH_32Bit.exe

Seeing as you are having no luck with the re-registration process....then I suggest making a copy of the one being used in the netbook. I would also make a copy of these to a DVD or flash drive for safe keeping.

-
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x2 seats]
Windows 10 - Quadro P2000