Cancel
Showing results for 
Search instead for 
Did you mean: 

no holes or thread database

Experimenter
Experimenter

Hello. I have a student version of Solid Edge ST9, and i just cant make a hole, or thread. But I need to make both, because I need it in a seminar work, and its my final class before diploma. So I would be very thankful for a solution.

 Untitled.jpgUntitled1.jpg

3 REPLIES 3
Highlighted

Betreff: no holes or thread database

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Pahert

 

 

 

what I can see in Your post is, that YOu seem to have ST9

 

from ST7 on there are only 64bit versions of SE available, so I can't imagine taht YOur programs folder will be within "Program Files (x386)" which is the 32bit folder

 

So I supose taht Your path to the holes database is set wrong.

 

Go to Settings - Options - File Locations and correct those entries (reset them to default)

 

20170630_1609.PNG

regards
Wolfgang

Betreff: no holes or thread database

Experimenter
Experimenter

Thank you for your help. It worked.Thank you!

Betreff: no holes or thread database

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Pahert

 

 

... welcome!

 

regards
Wolfgang