Cancel
Showing results for 
Search instead for 
Did you mean: 

no perpendicular

Phenom
Phenom

I received a 3D file (stl) from a bended plywood part.

 

I need to drill holes, perpendicular on the surface.

To do this I draw a scetch, perpendicular and create a surface 'Normal to curve'.

 

The only problem is, SE doesn't want to make the line perpendicular. I can work around by drawing a 2nd line and make this one tangent to the curve and the make the first line perpendicular to the tangent line.

 

So SE understands it all, it just doesn't want to do it...

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user
1 REPLY 1

Re: no perpendicular

Legend
Legend
I ran into this making lines perpendicular to a Bezier curve.
Using SE since V12, 2002
ST10 certified