Cancel
Showing results for 
Search instead for 
Did you mean: 

open old SE files with current SE ST5 Version Trail?

Not applicable
Hello!

I've tried to open *.par and *.dft files which are appr. 4 years old and I doesn't know from which version of SE.
I got a warning with following information:

The file you want to use was saved in a format which is not compatible with current used SE-Product.


Is there a way how to open that files?


Many thanks in advance!

BR
2 REPLIES

Re: open old SE files with current SE ST5 Version Trail?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Current versions of SE can most definetely open older versions, so that's not the issue. The message you are seeing is most likely the result of the files being created in a restricted license such as an academic license or the 45 day trial may be restricted from opening files created with a commercial license.
Where do these older files come from?


Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: open old SE files with current SE ST5 Version Trail?

Not applicable
Hello.
Thanks for the answer.
Now I understand this!