Cancel
Showing results for 
Search instead for 
Did you mean: 

ordered to synchronous in sheet metal

N/A

hi
i wanted to move some features which i did in ordered to synch but it been done below of three changes of bends (modify/rotate faces) in the tree, i can't put these changes validates in topo or above of three change angles, in ordered, and as you know when put to move the features select all that above; somebody help? It's urgent.. anything i'll post a print.

thanks

4 REPLIES

Re: ordered to synchronous in sheet metal

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
So what are you asking? If the features are dependent on the move/rotate faces then you will not be able to move them above them. You can check dependency by using the shortcut menu and selecting 'Show Parents/Children'. And as you already know... moving features to Synch requires all upper features to be moved as well.


Ken

Production: ST10 MP7
Testing: SE 2019
http://Grundey.blogspot.com

Re: ordered to synchronous in sheet metal

N/A
yes, i know, but i needed to move a cut out and a flange which i created after change the angle; any suggestion to get it or just making direct in the synch..
thanks (sorry if the english is bad..)

Re: ordered to synchronous in sheet metal

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Hi there,
Maybe you could upload the Solid Edge file....and someone with Student Edition handy could take look at it for you.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: ordered to synchronous in sheet metal

N/A
i use the st5 student edition.., but ok, i'll make in synch even..
thanks guys