Cancel
Showing results for 
Search instead for 
Did you mean: 

part to Sheetmetal Coversion new Funtion

Valued Contributor
Valued Contributor

hell edge users..

I have a series of questions ...
When you want to convert from part to sheet metal, it works well in the outward direction of the body,
An exclamation point appears inside. And not.
I am making a lot of sheet metal in the inside direction.
What is the reason for this?inner body.png

(When the picture above selects the body inside ..)

outer body.png

(This picture is for selecting the exterior of the body.)

If there is only one direction, why is there an arrow to select?

 

Have you experienced this experience?
How did you solve it?

 

file attach

 

8 REPLIES 8

Re: part to Sheetmetal Coversion new Funtion

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Hclee,

 

I would expect this to be related to the bend radius vs. material thickness, but also can be material collisions where relief would be.

Synchronous seems to convert it with no trouble, but Ordered requires a bit more tweaking.

 

 

Attached, is another way [using Ordered mode] I would convert an imported part file, then modify this for production.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: part to Sheetmetal Coversion new Funtion

Valued Contributor
Valued Contributor

Thank you for answer.
This is not one or two.
That's the part that needs improvement.

Betreff: part to Sheetmetal Coversion new Funtion

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @Hclee

 

 

 

works well here in a similar test situation

 

20170627_1043.PNG20170627_1044.PNG

regards
Wolfgang

Betreff: part to Sheetmetal Coversion new Funtion

Valued Contributor
Valued Contributor

Hi ~ hawcad
Did you use the file I attached?
Or did you draw it alike?
Can you capture options for cover to sheetmetal?

Betreff: part to Sheetmetal Coversion new Funtion

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee

 

 

my example was done by myself, but I also can switch Your model to both sides.

 

Outside:

20170627_1306.PNG

 

Inside:

20170627_1307.PNG

 

 

And the next question might be, why You don't use this functionallity for the complete sheet metal part?

You also can select those greater bend radii already existing to get the side walls too:

 

20170627_1308.PNG

 

 

regards
Wolfgang

Betreff: part to Sheetmetal Coversion new Funtion

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee

 

 

 

back and retou!

 

 

All bends and inwards doesn't work!

This makes problem in the connection area.

 

So what's about changing the model to the inside values and then creating the PSM outwards?

 

 

regards
Wolfgang

Betreff: part to Sheetmetal Coversion new Funtion

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee

 

 

 

and another way to get it:

 

"Just see the imported model You have used, which is a PSM only.

So I think those thickness, together with the sharp edges will disallow the convertion into PSM

 

So use the convert for the middle part of Your model and create a flange followed with a tab on the side

20170627_1326.PNG20170627_1327.PNG20170627_1328.PNG

regards
Wolfgang

Betreff: part to Sheetmetal Coversion new Funtion

Valued Contributor
Valued Contributor

Thank you .. haw cad
I want to convert to sheet metal at once.
Converting to some extent and using the sheet metal function again
This is not the direction I want to go.
First, I need to study more and find a way ...
I think the outside is inside, not inside and it is definitely wrong.