Cancel
Showing results for 
Search instead for 
Did you mean: 

pattern feature

Creator
Creator

can somebody show me complete process of pattern features in assembly?

I have 4 hole feature on one plate 

now i want to create linear pattern to create in second plate as you can see in picture.

When i try to do that with pattern feature,

I can only draw the rectangle 

that will create un-necessary holes.

2 REPLIES

Re: pattern feature

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

It's not clear what pattern you want but click on the pattern sketch, the black rectangle, whereupon a dialog will come up to set the pattern options.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Betreff: pattern feature

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Raumik

 

 

 

I hope I have understand Your request completely.

 

To create Your hole feature a second time for the second plate You have two possibilities.

 

Either You use a rectangular pattern (as wanted) but keep an eye onto the right pattern count numbers.

I see more than 2 green points on Your rectangle.

 

You need a pattern count of 2 for the long direction and a pattern count of 1 for the short.

 

 

Or You use a curve (linear) pattern created on the fligh with a fixed pattern type and the right distance

 

See video of the rectangular method:

 

 

regards
Wolfgang