Cancel
Showing results for 
Search instead for 
Did you mean: 

pattern of an embossed number increasing it automagically?

Experimenter
Experimenter

Hello everyone,

I need to create a circular pattern of embossed numbers, ranging from 01 to 50. is there any way to do this so the number increase for every pattern element?

So I start with 01 and the pattern will reproduce a 02, 03, 04... etc.

Thank you!

 

Francesco

1 REPLY 1

Re: pattern of an embossed number increasing it automagically?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi,

I do not think you can create this with pattern command, but maybe the Text profile can help you with this task. You have to manually define numbers and then you can wrap Text profile around a circle.

 

Ota

(view in My Videos)