picture in draft

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

I have created a label, in a part file I draw rectangle in a sketch where I inserted a picture. The label looks good in the part file. How can I make the picture to be shown in a draft file, I only see the rectangle from the sketch and no picture. I selected Shaded with Edges from  Shading Options but does not show the picture. Waht other settings do I need to check?

 

Regards,

Marc

3 REPLIES

Re: picture in draft

Honored Contributor
Honored Contributor

I have a similar issues, but my picture is part of the material definition. I'n my case it's a bump map of expanded metal.

 

Modeling expanded metal is way to file size heavy. The bumpmap looks great when modeling in draft, not as good.

 

The best way I have right now to display it with by using a shaded with grayscale display type in the draft environment. I try to minimize such display as that uses up the ink in the printer. But that only works for a representation of the finished part. I have yet to figure out how to show the expanded metal pattern in flat as the folding pattern is a function of the # of diamonds, not the dimension. And the diamond sizes are inconsistant.

Re: picture in draft

Esteemed Contributor
Esteemed Contributor

Hi Marc,

 

What you need to do, is create a "New" "Face Style" then on the "Texture" tab, place your decal image.....use "Part Painter" to place the image to a part, selecting the "face" section filter [or could use an offset surface] in my example I've chosen to use the "Split" [based on a sketch I'd placed] command, from the surfacing tab.

 

When displayed as "Shaded" in draft, the "New" face style will be displayed.

 

Note: You may need to tweek scale & rotation of the decal image to fit the face you select....but it's all just tweaks from the relevant options....let me know if you need further info.

 

 

SE_ST6_Part_FaceStyle.png

 

SE_ST6_Part_FaceStyle_DraftResult.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP2] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: picture in draft

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor
Thank you Sean, it works this way.