Cancel
Showing results for 
Search instead for 
Did you mean: 

please help

N/A

Dear Forum

My name is Mariano a Computer Aided Design student, thanks for you quick response with the downloading details, but unfortunately I haven’t been able to download the program, it takes a lot of time and when it gets to 70 and above it just says that downloading error and does it, and I try and try and the message keeps repeating, well it has gone the 24 hour validation period and I still try but the same message appear.

Please I need the program as soon as possible as I have so much work to do and due to the dead line I can possibly failed the subject.

Please anything you can help with, in order for me to download the program, will be much appreciated.

Kind Regards

Mariano Ospina Cadavid
LSBU London
ospinam4@lsbu.ac.uk

2 REPLIES

Re: please help

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Try to download through a different computer or, if you know someone that already has SE, ask him the installation files, as the only thing that is different is the license file.

Re: please help

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Mariano,

...try using an download manager, such as "Internet Download Manager", or you could use "Mozilla Firefox" instead of Internet Explorer. (if that is what you use)
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP7] Classic [x2 seats]
Windows 10 - Quadro P2000