Reply

printing

Hi all new to solid edge and having problems printing

as soon as i click on print i get a low memory error message and solid edge shuts down.

6 REPLIES

Re: printing

Hi there,

 

I guess the first thing to cover is, what are your system specs? [maybe you actually have low system memory]

Sean Cresswell
Design Manager Streetscape Limited
Solid Edge ST9 [MP3] Classic [x2 seats]
Windows 10

Re: printing

Hi Sean spec is windows 7 enterprise 64 bit, core i7 processor, 8gb ram, 300gb memory, intel hd graphics 3000, NVIDIA quadro 1000m.
When solid edge is open task manager shows plenty of memory. Doesn't seem to be low on memory.

Re: printing

[ Edited ]

The memory error could be misleading.

This could as well be a printer driver issue.

Hard to guess from the description since no information is given about the printer being used.

A printer driver update might help.

 

~Tushar

 

Re: printing

All other programs print fine so I would think driver is ok unless printer not compatible with solidedge.
the program closes before you choose a printer though

Re: printing

Hi there doesnt seem to be any shortage of memory when usinng solid edge.

I have played with then virtual memory settings but still not printing!

Re: printing

[ Edited ]

Can you do a screenshot (top bit) of the info Screen, you get this by holding Ctrl Alt and double clicking the 3rd mouse button. Will help. 

 

Are you using colour views. this has caused problems for me in the past. 

ST8 MP11 / ST9 MP02