Cancel
Showing results for 
Search instead for 
Did you mean: 

problem in 3D environment with solid edge ST9 (graphics isue?)

Experimenter
Experimenter

hi,

 

i recently installed solid edge ST9 student version and immediately after i've incounterd a major issue in the 3d environment. everytime when i start a new project or open an existing one the view gets all shattered, to be correct (sketches, surfaces and solids) the whole part actually gets messy.

 

Has someone dealt with the same issue before? 
2017-09-16.png

 

my laptop specs are...

* GeForce 940M

* Intelcore i5 @2.2GHz

* 16GB RAM

 

Thanks

 

2 REPLIES 2

Re: problem in 3D environment with solid edge ST9 (graphics isue?)

Siemens Phenom Siemens Phenom
Siemens Phenom

Download and install the latest Nvidia graphics driver.

Betreff: problem in 3D environment with solid edge ST9 (graphics isue?)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @yene

 

 

 

I have seen this very often with Gforce cards.

 

As @uk_dave mentioned first should be to update Your drive and second if this doesn't help change the graphics setting in SE from "Graphic Card Advanced"  to "Graphic Card"  only.

 

 

20170916_1731.PNG

regards
Wolfgang