Cancel
Showing results for 
Search instead for 
Did you mean: 

question about Harness module and setup SE v20

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

I have some question about Harness module in SE. (Currently what I Use is ST7 version)
I made 1 Assembly to test Harness Wizard and it was make wires automatically.
I was successfully make it and report, but the report has no information about bundle's length.
how can I extract it?
and I want to control wires, bundles, cables option.
I know Harness Wizard makes wires based on "SEHarness.txt", "Condoctors.txt" located ST7>Preference.
can I add there the other options what I want?

 

----------------------------------------------------

this is the other question.
I have License already, but I deleted Solid Edge setup file. I want to setup SE v20.
where Can I download Solid Edge v20?

1 REPLY 1
Highlighted

Re: question about Harness module and setup SE v20

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

don't know for V20

 

as per the wire harness report: you have to use 'harness report' (tool tab) then choose the 'connections' option and the 'format' button and finally add the column for the cut length.