Cancel
Showing results for 
Search instead for 
Did you mean: 

"Discover components" function need or work around.

Innovator
Innovator

Hello,

 

I have a file that I am importing from another program.

This file has the same component in it multiple times but in different places. 

This component is a simple sphere but it was created in an "art" modeling program so it has tons of faces.  I'd like to simplify it by replacing it with a simple sphere. 

 

These spheres (beads) make up a 3d sculpture

of a swan.  

 

In Keycreator (Cadkey), there is a command that finds

duplicate solids and replaces them all this the same part.  I keeps the same relative postition too.

 

Is there anyway to do this in SE?  when I "replace" component it move the position.  I want to keep the layout of the parts but have it be made of 1 part repeated. 

 

Thanks!

 

Steve
Tweeting @lussierinbox

Even the Longest journey starts
with a small step! Smiley Wink
9 REPLIES 9

Re: "Discover components" function need or work around.

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hello Steve:

 

I am not able to reproduce the problem you described.

Can you attach an image of the end result after replacing the spheres ?

See this video below if it helps: I tried this with an imported assembly as well and it worked fine.

 

 

~Tushar

Re: "Discover components" function need or work around.

Innovator
Innovator

Hmm I wonder what the difference is ?

 

Here is the file if you could try it for me that would be awesome!  thanks

 

 

In in RAR for to reduce the size.

 

Steve
Tweeting @lussierinbox

Even the Longest journey starts
with a small step! Smiley Wink

Re: "Discover components" function need or work around.

Innovator
Innovator

I think it is do to the origin placement in the imported part. 

 

The origin is offset in each part so the replacement doesn't match up.

 

 

Steve
Tweeting @lussierinbox

Even the Longest journey starts
with a small step! Smiley Wink

Re: "Discover components" function need or work around.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I was just going to suggest that the origin is the problem. It must be in the same position as the original model or else it will shift according to the offset when you do a replace.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: "Discover components" function need or work around.

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Right, occurrences show all zero values.

 

2016012002.png

Re: "Discover components" function need or work around.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Tushar, if these are the results from his original file wouldn't it follow that there would be no offset with a replace if the replacement spheres are also on 0,0,0?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: "Discover components" function need or work around.

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Bruce, I am with you on this and thinking about the issue whole day.

Irrespective of the method the assembly was modeled in the originating CAD program, multibody or assembly or single part, once imported into Solid Edge and recognized as an assembly, I expect each part to 'know' where it is standing or 'floating' in the 3D space wrt the Base coord sys.

 

Re: "Discover components" function need or work around.

Innovator
Innovator

Yes the coord's seems to be the issue.  I wish two things to make importing better.

 

1.  To be able to recognize that the same body it used in multiple places.  Even if it does recongnize the pattern behind it. 

2.  Have the Relative coord's from the center of the mass ane the origin. 

 

This would make import assemblies easier, for sure.

 

 

Steve
Tweeting @lussierinbox

Even the Longest journey starts
with a small step! Smiley Wink

Re: "Discover components" function need or work around.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

That is the way it's supposed to work.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200