Cancel
Showing results for 
Search instead for 
Did you mean: 

"None" Face Style Color?

Would anyone happen to know where I can find the face style color settings when material is set to "none?"

 

none.jpg

 

 

face style.jpg

 

 

David McMahon
Solid Edge 2019
HP Z2 Mini, Windows 10
5 REPLIES 5

Re: "None" Face Style Color?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @David_McMahon,

 

So do you want to keep the Material set to "None", but change the part?.....you could just use part painter to get that result, else, double click the material to edit it to something. [assuming it exists in the material library - although easy to create your own]

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: "None" Face Style Color?

Shawn,

 

Thanks, the issue is that I can't find the "none" style anywhere to get the color settings. I just wanted to make sure I wasn't missing something. Not a big deal - I was just curious.

David McMahon
Solid Edge 2019
HP Z2 Mini, Windows 10

Re: "None" Face Style Color?

Phenom
Phenom

There's a style called Model Default - I presume it's that?

Re: "None" Face Style Color?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@David_McMahon,

 

Actually, I think this is just from the template, where "there is no material assigned", not to be confused with a listing for a material called "None"....and carries the "Model Default" scheme, as @Alex_H says.

 

.....I have my templates setup to open in my most common material, + thickness & bend radius, when in sheet metal.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: "None" Face Style Color?

Alex,

 

Thanks, not sure why I did not see that. For others that may be curious, below is the face style setting:

 

model_default.jpg

David McMahon
Solid Edge 2019
HP Z2 Mini, Windows 10