Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

"Open draft" in 3d context menu

Valued Contributor
Valued Contributor

It would be nice to add a new item on context menu in par/asm environment, to open the draft of a certain par/psm/asm file directly from 3d, without the need to browse the file system or go to the data management/where used tab.

I guess it could not very difficult to hide in this command the "where used" function, if the fast search is enabled.

____________________________
http://www.stimarchetti.it
Design of automation
9 REPLIES 9

Re: "Open draft" in 3d context menu

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

The command can be added to the radial menu since context menu is not easily customizable.

Like the context menu the radial menu is available at the mouse cursor.

Re: "Open draft" in 3d context menu

Valued Contributor
Valued Contributor
Which command? Where used or open draft? My interest is to avoid the extra-clicks to open the "where used" dialog just to open the draft related to a certain 3d model. The command "open draft" actually exists in the data management tab but it works only if a vault system is in use.
____________________________
http://www.stimarchetti.it
Design of automation

Re: "Open draft" in 3d context menu

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

I focussed only on the context menu part or your question, hence suggested using the radial menu.

I have little or no knowledge about the Where Used and Open Drawing commands from the Data Management tab.

  

To answer your question in a bit 'off topic' sense, I meant using the 'Open Draft Macro' from a radial menu slot.

Betreff: "Open draft" in 3d context menu

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Alessandro

 

 

This function already is here with ST10 and setup of BiDM.

 

You will find it under the Data management tab on the left.

 

This button will let You directly open the according draft or -if there are more than one - show You a list to select from.

 

regards
Wolfgang

Betreff: "Open draft" in 3d context menu

Valued Contributor
Valued Contributor

Where is the button to open the draft directly? Cannot find it.

 

Immagine.png

 

 

____________________________
http://www.stimarchetti.it
Design of automation

Betreff: "Open draft" in 3d context menu

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

I don't have a vault system installed but the Open Drawing button is enabled. 

Betreff: "Open draft" in 3d context menu

Valued Contributor
Valued Contributor

Ok, after the setup of the vault, now the button works!

Thank you very much for suggestion!

Cattura.PNG

 

____________________________
http://www.stimarchetti.it
Design of automation

Betreff: "Open draft" in 3d context menu

Valued Contributor
Valued Contributor
Actually it dows not need a real valut system , it is enough to add the search directories to the SE Options.
____________________________
http://www.stimarchetti.it
Design of automation

Betreff: "Open draft" in 3d context menu

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Alessandro

 

 

I believe that two things needs to be defined correctly:

 

The entries in the FastSearch.txt which defines the folders for search n for drafts and the setup for Windows index services which will deliver faster results.

 

 

regards
Wolfgang