Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

"Replace Part" error. SE says they have the same name.

Valued Contributor
Valued Contributor

I got this message when attempting to replace a part. The part I am replacing with was created by using "Replace Part with Copy". I changed the file name, stored it in the same folder as the original part and the assembly. The part was created in the folder with the new name, but not placed in assembly, because I got this message. Now whenever I try to "Replace part" and select the new part, I get the same message. The parts DO in fact have different names, and everything is in the same folder.

 

Untitled.jpg

6 REPLIES 6

Re: "Replace Part" error. SE says they have the same name.

Valued Contributor
Valued Contributor

This may be related to this error, which is also nonsense because there is only one part with that name anywhere and it is in the same folder as the assembly. In other words, placing a part from folder A into an assembly from folder A yields this message.

 

Untitled.png

Re: "Replace Part" error. SE says they have the same name.

Phenom
Phenom

What are the actual filenames? 

 

Can you repeat this workflow if you start a new assembly in a folder somewhere else and add dummy part documents with the same names?

-Dylan Gondyke

Re: "Replace Part" error. SE says they have the same name.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Have you tried to fix this with "Revision Manager".....or possibly "Edit Links", although, the later has a UI in need of a serious overhaul, not saying RM is a whole lot better.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: "Replace Part" error. SE says they have the same name.

Valued Contributor
Valued Contributor

After examining the actual paths for these parts using occurence properties, I think the problem is due to the fact that our file server has had some workaround installed because they replaced a server and were unable to give it the same name and so now instead they redirect us now automatically. Honestly I don't remember details, you'd have to ask our Information Technology  Dept. But the fact is that now some of our older files do seem to have a different path (if you ask SE, anyway) than our new ones, even though it all looks the same to me.

I'm going to mark this one down as SOLVED and blame our IT department, like I do every day. That being said, I think there may be a way that SE could be fixed to have it ask the OS for the file path instead of using the location it remembers.

Re: "Replace Part" error. SE says they have the same name.

Valued Contributor
Valued Contributor

Good idea on the revision manager, I know because it crossed my mind as well (and good ideas are all I ever have).

 

Thanks guys, for looking into this for me.

Re: "Replace Part" error. SE says they have the same name.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@DGMCENGINEERING wrote:

Good idea on the revision manager, I know because it crossed my mind as well (and good ideas are all I ever have).

 

Thanks guys, for looking into this for me.


 

All good.....I'm struck with that same disposition, although, others may suggest I'm full of other matter than good ideas.  Robot LOL

 

I moonlight as our IT dept as well......a little jealous, I'd really like if it was someone else that gets the blame. Robot wink

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000