Cancel
Showing results for 
Search instead for 
Did you mean: 

"TRIM CORNER"

Gears Phenom Gears Phenom
Gears Phenom

Any specific reason trim corner in Sync doesn't work the same as ordered?  I recently updated to ST8 and just now noticed you can't hold left mouse and drag over two corners to trim or connect them.

-Craig
4 REPLIES 4

Re: "TRIM CORNER"

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hey there "Captain Hollywood"  Robot LOL

 

Finished being a film star already, now it's back to work, huh?  Robot wink

Not sure the reason, but yes, the selection process for trim is not the same across Synchronous vs. Ordered. I don't recall, were we able to do this in ST7 [& earlier] Synch sketches?

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: "TRIM CORNER"

Gears Phenom Gears Phenom
Gears Phenom

Lol.. Lots of catching up to do after two days in front of the camera!

I barely used Sync in ST7 so I'm unsure if it worked there or not.

-Craig

Re: "TRIM CORNER"

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

You must be locked to that sketch plane.

RMB on the sketch and choose Lock Sketch Plane.

LMGi
www.TLMGi.com

Re: "TRIM CORNER"

Gears Phenom Gears Phenom
Gears Phenom
Not quite sure how I've missed that.. Thanks @JasonTitcomb
-Craig